To find the cause of this noise peak, I tried a few adjustments to my prototype to investigate the effect on the output noise. for starters, this is the physical setup:
- increasing the input capacitance: with an additional 20p at the input the noise around 100kHz is slightly higher and the noise at higher frequencies is slightly lower, I expect due to a shift in the Fc of the TIA. The shape of the peak at 400kHz however does not change
- decreasing the input capacitance: I removed the photodiode and the shielding to minimize capacitance at the input node and other parasitic capacitances. The resulting noise is negligibly different from the noise graph given above.
- minimizing TIA output load: with subsequent stages disconnect, again nothing changes on the measured output noise
- checking a different channel: this design contains multiple separate channels. The noise figure of this channel shows the same noise peak, but at a different frequency:
Thank you in advance!