ADA4310-1, 4311-1 with sloped PD0, PD1

When using 4310-1 or 4311-1, with PD0 and PD1 pins taking values between 0V and whatever is considered logic high, does the amplifier behave reasonably? By that does it behave without going unstable or draining excessive current or requiring excessive time to go back to the normal operation or normal inactive state? I would expect the amplifier to limit the output voltage range (signal potentially clipped) or the output impedance increase or some other behaviors, but I'm ok with those, as long as the change is gradual/continuous and the operation is reasonable.

The motivation of this question is, what if PD0 and PO1 are tied together, bypassed by a capacitor and driven by a medium impedance drive so that the time constant of that RC is on the order of tens of milliseconds? Any related information and the equivalent internal circuits around PO0, PO1 pins would be appreciated.

Parents
  • 0
    •  Analog Employees 
    on Apr 23, 2018 10:19 AM

    Hi Ryuji,

    Thank you for your patience.

    PD0 and PD1 are digital (CMOS) pins with a threshold of 1.5 V. Going above or below the threshold voltage will trigger the part to change it's operating mode. It doesn't matter how much voltage you are at as long as it exceeds the threshold, it will trigger. And it takes 2us for it to change state. And no, it doesn't affect the parameters you mentioned above.


    Regards.

Reply
  • 0
    •  Analog Employees 
    on Apr 23, 2018 10:19 AM

    Hi Ryuji,

    Thank you for your patience.

    PD0 and PD1 are digital (CMOS) pins with a threshold of 1.5 V. Going above or below the threshold voltage will trigger the part to change it's operating mode. It doesn't matter how much voltage you are at as long as it exceeds the threshold, it will trigger. And it takes 2us for it to change state. And no, it doesn't affect the parameters you mentioned above.


    Regards.

Children
No Data