Dear Sir/Madam,
The AD4857-1 datasheet specifies that:
"THE EXPOSED PAD MAY BE CONNECTED TO GND OR VS."
Is this +VS or -VS?
I have split supplies.
Regards Joe
ADA4857-1
Production
The ADA4857 is a unity gain stable, high speed, voltage feedback amplifier with low distortion, low noise, and high slew rate. With a spurious-free dynamic...
Datasheet
ADA4857-1 on Analog.com
Dear Sir/Madam,
The AD4857-1 datasheet specifies that:
"THE EXPOSED PAD MAY BE CONNECTED TO GND OR VS."
Is this +VS or -VS?
I have split supplies.
Regards Joe
Hello,
This is -VS, you can confirm this in the Abs Max Rating.
Thanks and regards.
Hi,
Thank you. Are there any advantages/disadvantages connecting the exposed pad to GND or -VS.
ie. are there any leakage paths for GND etc
RegardsJoe
Hello,
The Exposed Paddle is primarily used for heat dissipation and it is usually connected to the lowest potential.
For Single supply, your -VS is connected to GND, and this is your lowest potential.
For Split supply, your -VS is the lowest potential.
You can check this link to see some advantages of having an Exposed Paddle.
Thanks.
Hi,
Thank you.
Regards Joe