Post Go back to editing

RF/High Speed Signal Prototyping

I'm trying to use the AD600 (as well as some other components, but the AD600 for now) in a a high speed application, but do not have circuit boards yet.  The part does not have an evaluation board, but I'm not sure if I can use the white/breadboard prototyping method with high speed signals.  Any help with prototyping the AD600 or high speed signal prototyping in general would be greatly appreciated.

Other parts that I will be using that I also could not find evaluation boards for include the OP400A, AD534, ADG201, OP270 & OP467.

Thanks!

  • Hi-

    I moved this question about the AD600 and other linear products to the Amplifiers community.  Someone here should be able to assist you.

    Regards,

    AndyR

    EngineerZone Community Manager

  • LaserENGR,

      My rule of thumb is anything over about 1 MHz is not suitable for the white breadboarding strips.

    There is too much capacitance between nodes.  You can do a quick pc board design, send the

    data file to one of the quick prototying houses, and get three to six boards back in less than one

    week for less than $100.

    Pin outs for singles/duals/quads are pretty much standardized, so you can get some generic

    op amp eval boards that would work with a lot of part numbers.

    Go to:  http://www.analog.com/en/evaluation-boards-kits/resources/index.html

    and select op amps.

    Harry

  • Hello,

    This may be your lucky day!

    I'm the applications engineer for the AD600 and I happen to have an unreleased eval board for thre AD600 SOIC wide body package. I have boards that will accept a socket, or that have the normal solder pad pattern. These are not built but I think I stll have the documentation describing the board. I also support the AD534 but I never made a board for that part. I don't su[pport the other parts but you might contact Mr. Reza Moghimi to see if the amplifier group has a universal eval board for an 8-pin op-amp pattern.

    If all the parts you mentioned are on the same circuit you would be better off making a small circuit as HArry suggested, rather than bolting together several eval boards.

    best,

    js

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.