AD8067
Production
The AD8067 FastFET™ amp is a voltage feedback amplifier with FET inputs offering wide bandwidth (54 MHz @ G = +10) and high slew rate (640 V/µs). The...
Datasheet
AD8067 on Analog.com
Hello!
I've selected AD8067 as a high speed Op Amp.
Schematic is quite usual and shown below
Power is dual, +/- 3 V.
I have output pulse form like shown below
Blue plot is for input and yellow is for output.
It is the most clear output signal, that I can get by R3 adjustment.
What can be the reason of such distorsion?
Thank you for answer!