Hi,
I would like to know the common mode voltage range of ADA4522-2. I am using this as a buffer. The supply voltage to the Op-Amp is ±5 V and my input would be near to 5V( assume 4.9V). What can be my possible output value.?
Thanks in advance.
ADA4522-2
Recommended for New Designs
The ADA4522-1 / ADA4522-2 / ADA4522-4 are single/dual/quad
channel, zero drift op amps with low noise and power, ground
sensing inputs, and rail-to-rail...
Datasheet
ADA4522-2 on Analog.com
Hi,
I would like to know the common mode voltage range of ADA4522-2. I am using this as a buffer. The supply voltage to the Op-Amp is ±5 V and my input would be near to 5V( assume 4.9V). What can be my possible output value.?
Thanks in advance.
Hi Harry,
I am changing the resistors also to 0.1% tolerance with 25ppm/C. I feel this would reduce the change in resistance effects on temperature.
Regards,
Ashok
Hi Harry,
I am changing the resistors also to 0.1% tolerance with 25ppm/C. I feel this would reduce the change in resistance effects on temperature.
Regards,
Ashok