Hi,
I would like to know the common mode voltage range of ADA4522-2. I am using this as a buffer. The supply voltage to the Op-Amp is ±5 V and my input would be near to 5V( assume 4.9V). What can be my possible output value.?
Thanks in advance.
ADA4522-2
Recommended for New Designs
The ADA4522-1 / ADA4522-2 / ADA4522-4 are single/dual/quad
channel, zero drift op amps with low noise and power, ground
sensing inputs, and rail-to-rail...
Datasheet
ADA4522-2 on Analog.com
Hi,
I would like to know the common mode voltage range of ADA4522-2. I am using this as a buffer. The supply voltage to the Op-Amp is ±5 V and my input would be near to 5V( assume 4.9V). What can be my possible output value.?
Thanks in advance.
I would guess that the majority of your drift over temp comes from the resistors, especially R3. Is it a precision
resistor with a guaranteed tempco of less than 5 ppm/C??
Harry
I would guess that the majority of your drift over temp comes from the resistors, especially R3. Is it a precision
resistor with a guaranteed tempco of less than 5 ppm/C??
Harry