Post Go back to editing

What is the Common mode voltage range of ADA4522-2 ?

Hi,

I would like to know the common mode voltage range of ADA4522-2. I am using this as a buffer. The supply voltage to the Op-Amp is ±5 V and my input would be near to 5V( assume 4.9V). What can be my possible output value.?

Thanks in advance.

Parents
  • FormerMember
    0 FormerMember
on Mar 1, 2017 5:36 PM

C4 is BAD!!!  Remove it!!    If the op amp is a perfect voltage source, then the cap does nothing.

But op amps have a finite output impedance, so you create an R-C low pass which

gives phase shift and reduces stability, leading to oscillations.

Harry

Reply
  • FormerMember
    0 FormerMember
on Mar 1, 2017 5:36 PM

C4 is BAD!!!  Remove it!!    If the op amp is a perfect voltage source, then the cap does nothing.

But op amps have a finite output impedance, so you create an R-C low pass which

gives phase shift and reduces stability, leading to oscillations.

Harry

Children
No Data