Post Go back to editing

What is the Common mode voltage range of ADA4522-2 ?

Hi,

I would like to know the common mode voltage range of ADA4522-2. I am using this as a buffer. The supply voltage to the Op-Amp is ±5 V and my input would be near to 5V( assume 4.9V). What can be my possible output value.?

Thanks in advance.

Parents
  • Hi Ashok,

    Thank you for this information.

    When you say you are encountering issue in precision, do you mean you have a target accuracy that doesn't met or the circuit  doesn't functioning well?

    If you are using the uA747 with supply voltage of +/-5V and input voltage of 5V, I would expect that your circuit will not work.

    Clearly, based on your conditions, you really need a rail to rail input/output amplifier for it to work properly.

    I would recommend to use one of our rail to rail input/output amplifier which is the ADA4091-2.

    This was also used in some of our reference circuit for this kind of application which you can see here.

    Let me know if you need anything else.

    Best regards,

    Emman

Reply
  • Hi Ashok,

    Thank you for this information.

    When you say you are encountering issue in precision, do you mean you have a target accuracy that doesn't met or the circuit  doesn't functioning well?

    If you are using the uA747 with supply voltage of +/-5V and input voltage of 5V, I would expect that your circuit will not work.

    Clearly, based on your conditions, you really need a rail to rail input/output amplifier for it to work properly.

    I would recommend to use one of our rail to rail input/output amplifier which is the ADA4091-2.

    This was also used in some of our reference circuit for this kind of application which you can see here.

    Let me know if you need anything else.

    Best regards,

    Emman

Children
No Data