Post Go back to editing

About supply voltage of ADA 4310-1 (II)

I asked a question about this matter once.   https://ez.analog.com/thread/98682
Please allow me to ask you again.

Operating Range (Single Supply): +5 to +12 [V]
ABSOLUTE MAXIMUM RATINGS Supply Voltage: 12V

I have confirmed that you can use ± 3% of your 12V power supply, and is safe up to ± 5%.

I think that ADA 4310 - 1 is very similar to ADA 4311 - 1.
ADA 4311 - 1 has an absolute maximum rating of 13.6 V with respect to POWER SUPPLY (Single Supply) = 12 V.
Maybe, is ADA4310-1 also equivalent absolute maximum rating?

Best regards