Hello,
My question is if I can supply the AD8572 with positive sources 5v (pin V+) and negative voltage 5v (pin V-).
Thanks,
akarko01
AD8572
Production
This family of amplifiers has ultralow offset, drift, and bias current. The AD8571, AD8572, and AD8574 are single, dual, and quad amplifiers, respectively...
Datasheet
AD8572 on Analog.com
Hello,
My question is if I can supply the AD8572 with positive sources 5v (pin V+) and negative voltage 5v (pin V-).
Thanks,
akarko01
HI,
Generally, operational amplifiers can be configured at single supply and dual supply operation as long as the difference between the supplies are kept within the specification given in the datasheet. Unfortunately, AD8572 was only specified at voltages 2.7V and 5V which are below your 10V voltage specification, exceeding the abs. max value which is 6V.
May I know what your application is? Perhaps we can suggest a more suitable part for you.
Regards,
Goz