Post Go back to editing

ADCMP580 CML Output interfacing to +2.5V

Is it possible to connect the ADCMP580 directly to a +2.5V CML 1:2 fan-out driver or I need to add a level shifter in between? I need DC Coupling. One way this could be achieved is by connecting Pin 9 to the +V however I am not sure if internally Pin 9 and Pin 12 are connected to the GND?

I noticed this IC uses -V CMl which is very inconvenient to use with most of the available CML logic chips. Is there a solution which uses +V CML 2.5/3.3V?

Many Thanks,

Tom



Pin 9 comment
[edited by: rv27 at 11:31 AM (GMT 0) on 21 Jan 2020]
Parents
  • Hi,

    ADCMP580 CML output is from -350mV to 30mV so connecting it to a 2.5V would not be straight forward approach. Pins 9 and 12 are internally connected and can be a digital ground/positive logic supply pin but in the case of ADCMP580 proper termination to gnd with 50 ohms is necessary for proper return.

    If you want a comparator with CML output referenced to +V, you can check ADCMP606.

Reply
  • Hi,

    ADCMP580 CML output is from -350mV to 30mV so connecting it to a 2.5V would not be straight forward approach. Pins 9 and 12 are internally connected and can be a digital ground/positive logic supply pin but in the case of ADCMP580 proper termination to gnd with 50 ohms is necessary for proper return.

    If you want a comparator with CML output referenced to +V, you can check ADCMP606.

Children