Post Go back to editing

Data with regards to Output impedance for AD8029

Hi, 

Is there any data with regards to change in output impedance on change in output voltage .

Thanking you 

With best regards and wishes 

Parents
  • Hi Kabekami,

    Output Impedance is a frequency-dependent parameter of an op-amp. See figure 43 and 45 of AD8029's datasheet.

    In terms of change in output voltage, one parameter that you must consider the amplifier's output current drive. This parameter will be critical when the load is low, ILoad = Vout/RLoad. When Vs=5V, Isc=60 mA, this will limit the drive capability of the amplifier.

    Regards,

    Jino

Reply
  • Hi Kabekami,

    Output Impedance is a frequency-dependent parameter of an op-amp. See figure 43 and 45 of AD8029's datasheet.

    In terms of change in output voltage, one parameter that you must consider the amplifier's output current drive. This parameter will be critical when the load is low, ILoad = Vout/RLoad. When Vs=5V, Isc=60 mA, this will limit the drive capability of the amplifier.

    Regards,

    Jino

Children
No Data