Hi,
Is there any data with regards to change in output impedance on change in output voltage .
Thanking you
With best regards and wishes
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
AD8029
Production
The AD8029 is a single, rail-to-rail input and output high speed amplifier with a quiescent current of only 1.3 mA per amplifier. Despite its low power...
Datasheet
AD8029 on Analog.com
Hi,
Is there any data with regards to change in output impedance on change in output voltage .
Thanking you
With best regards and wishes
Hi Kabekami,
Output Impedance is a frequency-dependent parameter of an op-amp. See figure 43 and 45 of AD8029's datasheet.
In terms of change in output voltage, one parameter that you must consider the amplifier's output current drive. This parameter will be critical when the load is low, ILoad = Vout/RLoad. When Vs=5V, Isc=60 mA, this will limit the drive capability of the amplifier.
Regards,
Jino