Post Go back to editing

AD7667 input question

hi all:

      Looking at the AD7667 datasheet, I have troubles understanding Figure 45. Using the AD7667 in 16-Bit Bipolar and/or Wider Input Ranges.

Why the op amp can convert  ±10V to 0-2.5V. Should U2 connect the analog input signal to R2 and R3? But the gain is not right.

thanks

Parents Reply
  • Hi,

    In fact, to input connect the reference voltage, not R3. U2 provide calibration or autozero mode. In datasheet says about this: "When desired, accurate gain and offset can be calibrated by acquiring a ground and voltage reference using an analog multiplexer (U2), as shown in Figure 45".

    Regards,

    Kirill

Children
No Data