Post Go back to editing

Ad8610 Spice model

Is there an issue with the AD8610 spice model?

When I compare the ADA4610, AD8625 and AD8610, the output (Vout3) of the 8610 is heavily dependent on the input resistor R14.

For 1K or higher the output goes to the -rail.

This occurs when using +- 10V rails (as the design will be implemented)

If i change the rails in the model to +-13V the problem does not occur.

Thanks

Brendan

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.