We have used the LTC6240HVHS5#PBF variant of the LTC6240 in a circuit that measures voltage, with circuitry that changes the gain of the opamp depending on the circumstances. However, some of the units exhibit faulty behavior, including railed output far below the spec and extreme temperature sensitivity. These units include both ones that came back "from the field" and at least one that had never been used, from the PCB assembler.
Attached is a scope shot of a malfunctioning opamp in voltage follower configuration, isolated from the rest of the circuit. Yellow is V+, Green is the signal to the non-inverting terminal, blue is the output (V- is ground). The opamp starts to rail ~700mV below the rail.
When cooling the malfunctioning opamp in the scope shot to around -30C in this configuration, the opamps rail high at a lower input voltage. When heated to 100C, the opamp nearly returns to linear operation.
We were not able to "break" a working opamp in a lab setting by heating and cooling the opamp repeatedly while in operation. Replacing the bad opamp with a known working one allows the circuit to function properly, and moving the bad opamp to a known working circuit causes the circuit to malfunction. Among other tests, we can trace the cause of the malfunctioning circuit to the opamp.
Are there any known issues or defects with the LTC6240 with regards to temperature or other conditions? Could these symptoms be cause by relatively high vibration environments?
Thanks
uploaded new screenshot
[edited by: greg_soe at 8:40 PM (GMT 0) on 23 Jul 2019]