Post Go back to editing

Using ADA4350 evaluation board for high gain with photodiode.

I am looking to use the user defined feedback path of the ADA4350 evaluation board in order to amplify my photodiode signal which is detecting exponentially decaying fluorescence from a magneto-optical trap. 

My requirements are a gain of around 1 MOhm and a BW of around 20 kHz. Due to constraints on the collection optics and therefore photodiode active area my choice of input parameters are approximately CD = 9-18 pF, in order to ensure the lowest possible dark current. Because of the high feedback resistor required I presumed that I would need to use the T network in order to achieve a stable output. However I see no capacity to implement this on the board. Could you please give me advice on how to approach this?

Secondly, the datasheet states a GBWP of 175 MHz. However, I think Fig. 72 (or even Figs. 62-65) of the data sheet implies GBWP on the order of 1010 for a gain and frequency response that I would like to achieve. Have I misunderstood something in this section?

Looking forward to your reply.

  • Hi,

    Its hard if not impossible to configure the T network in the ADA4530 evaluation board, however, if you require a gain of 1M and BW of 20kHz, I think you could try a similar configuration in Figure 71, the parallel feedback combination of 1Mohms and 0.5pF. You just need to compute for Cf using equation 8 in page 32. The 175MHz is the GBW of the internal FET amplifier used. The Figures 62-65, tell you about transimpedance amplifier bandwidth which is equal to 1/2piRfCf.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.