Hi,
My customers are considering AD 8602.
So I got a question.
Is a protective diode etc. in the Input & output stage of the AD8602?
If voltage is applied to Input when power supply is not being applied to the AD8602,
I am concerned about whether the input terminal and the output terminal are satisfactory.
In the "Input Overvoltage Protection" section of the datasheet, there is a method of limiting the input current,
and if this method is used it will not damage the amplifier, but if this method, also damage on the output side
Is not there a problem with the recognition that it does not give?
Best regards,
Yuya