Hello,
I am using the ADA4807 model to model the ADA4807-2 in an active filter application where the output is a 10 MHz sinewave. The output has a peak voltage of 1.79 V.
Theoretical calculation shows:
Min Req Slew Rate = 2 * pi * 10 * f * Vpeak/(10^6) V/us
Which gives minimum 112 V/us slew rate to avoid distortion for this application.
The datasheet states that the ADA4807/ADA4807-2 has a 225 V/us slew rate, but significant slew rate distortion appears in simulation:
Blue is input waveform, red is output.
Is this an error in the spice model?
Thanks!