AD817
Production
The AD817 is a low cost, low power, single/dual supply, high speed op amp which is ideally suited for a broad spectrum of signal conditioning and data...
Datasheet
AD817 on Analog.com
I Have AD817.cir from analog site, but I have no idea how to use it on LTspice?
there is whats inside it:
* AD817 SPICE Macro-model
* Description: Amplifier
* Generic Desc: High Speed, Low Power Wide Vs Op Amp
* Developed by: ARG / ADI
* Revision History: 08/10/2012 - Updated to new header style
* 1.0 (11/1992)
* Copyright 1993, 2012 by Analog Devices, Inc.
*
* Refer to www.analog.com/.../spice_general.html for License Statement. Use of this model
* indicates your acceptance with the terms and provisions in the License Statement.
*
* BEGIN Notes:
*
* Not Modeled:
*
* Parameters modeled include:
*
* END Notes
*
* Node assignments
* non-inverting input
* | inverting input
* | | positive supply
* | | | negative supply
* | | | | output
* | | | | |
.SUBCKT AD817 2 1 99 50 46
*
* INPUT STAGE AND POLE AT 160MHZ
*
I1 8 50 1E-3
Q1 4 1 6 QN
Q2 5 3 7 QN
CIN 1 2 1.5PF
R1 99 4 1.188K
R2 99 5 1.188K
C1 4 5 4.187E-13
R3 6 8 1.137K
R4 7 8 1.137K
IOS 1 2 12.5E-9
EOS 3 2 POLY(1) (15,98) 0.5E-3 10
*
* GAIN STAGE AND DOMINANT POLE AT 8.8KHZ
*
EREF 98 0 POLY(2) (99,0) (50,0) 0 0.5 0.5
G1 98 9 (4,5) .8415E-3
R5 9 98 5.942E6
C2 9 98 3.045E-12
D1 9 10 DX
D2 11 9 DX
V1 99 10 1.83
V2 11 50 1.83
*
* COMMON MODE STAGE WITH ZERO AT 3.16KHZ
*
ECM 14 98 POLY(2) (1,98) (2,98) 0 0.5 0.5
R7 14 15 1E6
C4 14 15 5.036E-11
R8 15 98 1
*
*POLE AT 120MHZ
*
GP2 98 31 (9,98) 1E-6
RP2 31 98 1E6
CP2 31 98 1.326E-15
*
*ZERO AT 60MHZ
*
EZ1 32 98 (31,98) 1E6
RZ1 32 33 1E6
RZ2 33 98 1
CZ1 32 33 2.65E-15
*
*ZERO AT 100MHZ
*
EZ2 34 98 (33,98) 1E6
RZ3 34 35 1E6
RZ4 35 98 1
CZ2 34 35 1.59E-15
*
*POLE AT 120MHZ
*
GP3 98 36 (35,98) 1E-6
RP3 36 98 1E6
CP3 36 98 1.326E-15
*
*POLE AT 160MHZ
*
GP10 98 40 (36,98) 1E-6
RP10 40 98 1E6
CP10 40 98 .995E-15
*
* OUTPUT STAGE
*
RO1 99 45 16
RO2 45 50 16
G7 45 99 (99,40) 62.5E-3
G8 50 45 (40,50) 62.5E-3
G9 98 60 (45,40) 62.5E-3
D7 60 61 DX
D8 62 60 DX
V7 61 98 DC 0
V8 98 62 DC 0
GSY 99 50 (99,50) 7.692E-6
FSY 99 50 POLY(2) V7 V8 5.77E-3 1 1
D9 41 45 DX
D10 45 42 DX
V5 40 41 0.04
V6 42 40 0.04
LO 45 46 .06E-9
*
* MODELS USED
*
.MODEL DX D
.MODEL QN NPN(BF=151.52)
.ENDS
Hi,
Download the AD817.cir file from Analog site.
Open it using your LTspice program.
Point on the line where the ".subckt" line and right click on it to create symbol.
The box symbol created is located on the "Auto-generated" library in LTspice.
Hope this helps.
Hi,
Download the AD817.cir file from Analog site.
Open it using your LTspice program.
Point on the line where the ".subckt" line and right click on it to create symbol.
The box symbol created is located on the "Auto-generated" library in LTspice.
Hope this helps.
Thanks, But how to change and make our own shape for it's symbol? Is there any reference?
And do you have any idea, why the model not works correctly?

this is RtoR but it clamps!!!
Hi,
Unfortunately, ADA4851spice model have some problem.
What application are you working on? Maybe we could give you some advice based on that on what part to select.
What particular parameter are you concerned?
Right now, your option is to just choose other part spice model closed to ADA4851 depending upon your application.
any idea?
I have same issuer with ADA8282 can you please verify if that is correct?
ez.analog.com/.../ada8282-spice-model-failure
Hi,
I posted a reply to your original question about ADA8282 model, link below:
Regards,
Hooman