I don't see the AD8063 listed in the LTspice amplifier menu. What are my options? Is there a similar device I can import?
Thanks,
Jason
AD8063
Production
The AD8061/AD8062/AD8063 are rail-to-rail output voltage feedback amplifiers offering ease of use and low cost. They have a bandwidth and slew rate typically...
Datasheet
AD8063 on Analog.com
I don't see the AD8063 listed in the LTspice amplifier menu. What are my options? Is there a similar device I can import?
Thanks,
Jason
Hi,
What is your application?
Why you initially choose AD8063?
The application involves level shifting and amplification of analog NTSC/RS170 video, including output buffering to cables. I chose the AD8063 based on cost, performance and output range/drive.
More specifically, powering the amps at either +5/0V or +3.3/-1.7V (board option) and buffering/level shifting (G=1) or amplifying (G=2) 1.5Vp-p max input signal where the input and output are always at least 0.5V from either rail.
I am closing this since I was able to simulate the AD8063 using ADIsimPE. There was an issue with the model but ADI confirmed that this part would do what I needed and it has been working great on the finished product.