Hi,
My customers are considering ADA 4817-1.
So I got a question.
It is about operation in the Power Down state.
#1 Is the input pin High-Z (high impedance)?
#2 Does the current leak from the input pin?
Best regards
Yuya
ADA4817-1
Production
The ADA4817-1 (single) and ADA4817-2 (dual) FastFETâ„¢ amplifiers are unity-gain stable, ultrahigh speed, voltage feedback amplifiers with FET inputs....
Datasheet
ADA4817-1 on Analog.com
Hi,
My customers are considering ADA 4817-1.
So I got a question.
It is about operation in the Power Down state.
#1 Is the input pin High-Z (high impedance)?
#2 Does the current leak from the input pin?
Best regards
Yuya
Hi Yuya,
During power down state,
The leakage current at the power down pin is indicated in the ADA4817-1's datasheet.
Typically 34uA at ±5V operation.
and typically 31uA at 5V operation.
But if you're referring to the amplifier's input (+IN and -IN), It's always in High-Z and the Input bias current are still present and specified on the datasheet.
Typically 75pA at ±5V operation.
and typically 50pA at 5V operation.
Best Regards,
Dann