Hello!
The datasheet of ADA4522 shows the measured voltage noise density for only > 10 Hz frequency region.
I was measured the power spectral density (square of voltage noise density) in the 0.001-32 Hz range.
The result is shown at the attached figure.
OPAMP was configured as non-inverting with the 100 Ohm and 10 kOhm resistors (both 0.01 %).
The "+" pin was shorted to ground.
The PCB layout was as in the following article
(figure 13) to minimize the thermoelectric voltages. Extra "dummy" resistor at the "+" input was added and set to 0 Ohm or to Rg||Rf.
The PCB was placed into the Faraday box, which placed into the styrofoam box with no airflows.
The record of 55 hours length was obtained, and the periodograms width the 2000 seconds rectangular window was averaged.
The questions are:
1) Does ADI have the such extended Voltage Noise Density measurements, say - down to 0.1, 0.01 and 0.001 Hz?
2) The estimated white noise ASD = sqrt (49) = 7 nV / sqrt (Hz) is some higher than was expected for this configuration
(see green line level at the figure). Is it correct result?
3) The expected corner frequency was about 0.005 Hz, where the white noise level intersects the noise floor of the measuring system.
However, the ~0.1 Hz corner frequency was obtained.
Is this corner frequency intrinsic to the ADA4522 OPAMP? If so, is the ADA4528 OPAMP has the similar behavior?
Or the corner frequency obtained still relays to the uncompensated thermoelectric voltages?
Thank you in advise,
Peter.
Simultaneous noise measurement of the ADA4522 and the ADA4528 opamps, mounted on the same PCB. Common bipolar power supply +- 2.5 V. The PCB mounted as described above. Gain set to 1001 (10 and 10000 Ohms SMD 0602 1% resistors).
A new picture added.
[edited by: TPeter at 3:27 PM (GMT -5) on 11 Nov 2018]