Hello,
I've used spice model of AD8657 on LTspice. Then I get 40mV offset voltage between the inputs of AD8657 by .op analysis. Is the model correct? When I used the spice model of AD824, the offset voltage is around 40uV.
Best regards,
Akira
AD8657
Production
The AD8657/AD8659 are dual and quad micropower, precision,
rail-to-rail input/output amplifiers optimized for low power and wide operating supply voltage...
Datasheet
AD8657 on Analog.com
AD824
Production
The AD824 is a quad, FET input, single supply amplifier, featuring rail-to-rail outputs. The combination of FET inputs and rail-to-rail outputs makes the...
Datasheet
AD824 on Analog.com
Hello,
I've used spice model of AD8657 on LTspice. Then I get 40mV offset voltage between the inputs of AD8657 by .op analysis. Is the model correct? When I used the spice model of AD824, the offset voltage is around 40uV.
Best regards,
Akira
Hi,
Can you attach your test circuits? That would be helpful in analyzing your issue. Thanks.
Regards,
Arthur
Hi Akira,
I had a quick run of AD8657 and AD824 DC parameters on LTSPICE, both offset voltage are within the datasheet spec which is 350uV for AD8657 and 100uV for AD824.
Please see below for my test setup and simulation results.
We usually model and characterize the amplifiers on the highest supplies available on the spec table. I recommend using +/- 9V on AD8657 and +/-2.5V on AD824.
Please try this on your simulation and let me know if we get the same results.
Best Regards,
Dann
Hi Dann,
Thank you for your answer. I confirmed it and got the same results.
Thanks & regards,
Akira
Sorry, it's late.
If I take +5V and -5V for power then i get -19.053629mV
Is this O.K.?
Best regards
Fritz2
Hello Fritz2,
Please refer to the following questions:
1. Did you also used AD8657?
2. Is -19.053629mV the input offset voltage that you have measured?
3. How did you measure the input offset voltage? Do you have a schematic that you can share?
Having the above data will surely help us proceed with your question. Thank you very much.
Best regards,
Paul