Hi to everyone,
I'm an electronic engineering student, I'm trying to simulate the model in the object in transient analysis but, even if I downloaded the model you published as answer to previuos discussions, I'm still getting the problem "Node U1:U4_N24227 is floating and connected to current source G:U1:_U4_G4". I'm just trying with a DC signal. Can you help me? Maybe there is a mistake in my circuit or a problem in the model. The circuit is the following.
The simulation report is this one:
ERROR: Node U1:U4_N24227 is floating and connected to current source G:U1:_U4_G4
Direct Newton iteration failed to find .op point. (Use ".option noopiter" to skip.)
Starting Gmin stepping
Increasing initial diagonal Gmin to 100
Increasing initial diagonal Gmin to 1000
Increasing initial diagonal Gmin to 10000
Increasing initial diagonal Gmin to 100000
Increasing initial diagonal Gmin to 1e+006
Initial Gmin=1e+006 failed
Gmin stepping failed
Starting source stepping with srcstepmethod=0
Source Step = 3.0303%
Source Step = 21.2595%
vernier = 0.00390625
Starting source stepping with srcstepmethod=1
Source Step = 3.0303%
Source Step = 21.2595%
vernier = 0.00390625
Source stepping failed
Pseudo Transient failed in finding the operating point at 5 µs.
Trouble finding operating point....skipping operating point for Transient analysis.
Ignoring empty pin current: Ix(u1:pwra)
Ignoring empty pin current: Ix(u1:vcom)
Changing Tseed to 1.95312e-011
Changing Tseed to 1.95312e-013
Changing Tseed to 1.95312e-010
Changing Tseed to 1.95312e-014
Changing Tseed to 1.95312e-009
Changing Tseed to 1.95312e-015
Changing Tseed to 1.95312e-008
Changing Tseed to 1.95312e-016
Changing Tseed to 1.95312e-007
Changing Tseed to 1.95312e-017
Changing Tseed to 1.95312e-006
Changing Tseed to 1.95313e-018
to 3.90625e-018
Heightened Def Con from 3.90625e-018 to 2.6258e-017
Date: Fri Jul 24 20:58:26 2020
Total elapsed time: 0.664 seconds.
tnom = 27
temp = 27
method = modified trap
totiter = 19533
traniter = 2512
tranpoints = 1130
accept = 1101
rejected = 386
matrix size = 70
fillins = 10
solver = Normal
Thread vector: 8.6/5.8[2] 1.3/1.7[1] 5.1/2.0[2] 0.3/1.3[1] 2592/500
Matrix Compiler1: 2.43 KB object code size 0.8/0.4/[0.3]
Matrix Compiler2: 5.00 KB object code size 0.9/1.3/[0.6]