OP37: FAQ

  • Created
  • Updated
Was this helpful?
  • ADA4637-1 and OP37 pin compatibility in SOIC

    Question Are ADA4637-1 and OP37GSZ in SOIC package pin compatible? Answer ADA4637-1 and OP37GSZ, are not pin compatible. But if you can externally short pin 5 and 8, then they become pin compatible.
  • OP37: Reversal of supply voltage

    Question I have had a query from a customer they have wired an OP37 incorrectly. Instead of +15V and 0V they have applied -6V on the V+ pin and +5V on the V- pin, the parts were then powered up and…
  • radiation effect on OP37

    Question Are there any documents on the effect of neutron and gamma radiation on op37? Answer Please find attached Total Ionizing Dose (TID) Test Reports for OP37.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.