Post Go back to editing

ESD Ratings and Qualification Data

Category: Datasheet/Specs
Product Number: ADA4254

Hi,

 

We are currently carrying out a schematic review of a design using the ADA4254 instrumentation amplifier and require confirmation of its ESD ratings.

 

I have reviewed the ADA4254 datasheet, including the ESD map in Figure 85, which shows the internal protection circuitry. However, I cannot find any specified ESD withstand voltage.

 

Could you please confirm the following:

 

  1. The ESD rating for the Human Body Model (HBM) and Charged Device Model (CDM).
  2. Whether the device has been tested to IEC 61000-4-2, and if so, the contact and air discharge ratings.
  3. Whether any additional external protection is recommended for the analogue inputs to meet 8 kV contact and 15 kV air discharge requirements.

 

If available, could you also provide any relevant ESD qualification or test reports to support our design review?

 

Thanks for your help.

 

Best regards,

Eugene

Ref 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.