Post Go back to editing

Strain Gauge Amplifier with Gain of 4500

Thread Summary

The user seeks to amplify a strain gauge bridge signal with a gain of 4500 using the AD8237, which has a max gain of 1000. The final answer suggests that while the gain can be increased beyond 1000, performance is not guaranteed. Alternative amplifiers like AD8421, AD8429, and AD8222 are recommended, or an additional gain stage using a precision op-amp can be added to achieve the desired gain.

View FAQ
AI Generated Content
Category: Hardware
Product Number: AD8237

Hi, 

I have used the AD8237 for amplification of a strain gauge bridge already. While it worked fine in one sensor application, I have to adapt this now to a sensor with very low sensitvity. In fact the bridge output signal must be amplified round about with a gain of 4500 to match output signal to torque input (V/Nm). 

The max. Gain given in the datasheet is 1000, thus I think "just" increase the gain setting resistor "R2" acc. datasheet.. This would by calculation result in higher Gain, but I assume there is a reason to limit the gain setting to 1000, isn't it?

Is there another amplifier better to be used for this high Gain also including similar offset adjustment?

Thanks a lot and KR

Parents
  • Hi  ,

    Good day. The datasheet specification for gain range shows that it is characterized or guaranteed on the min and max gain range. But I agree that you can use the calculation on gain to set it beyond the specified max gain of 1000. But, take note that the parts performance is not guaranteed beyond gain of 1000 and therefore some specs may vary for the part. 

    For higher gain, I would also recommend that you consider AD8421, AD8429 and AD8222 but these amplifier does not similar offset adjustments. However, all of this amplifiers had reference pin at which you can use to adjust the output based on the DC offsets. Also, you can also consider adding an additional gain stage after the AD8237 to achieve the gain of 4500 (Gain of 1000 for AD8237 + Gain of 45 using an precision op-amp).

    Thank you.

    Regards,
    Gilbeys 

Reply
  • Hi  ,

    Good day. The datasheet specification for gain range shows that it is characterized or guaranteed on the min and max gain range. But I agree that you can use the calculation on gain to set it beyond the specified max gain of 1000. But, take note that the parts performance is not guaranteed beyond gain of 1000 and therefore some specs may vary for the part. 

    For higher gain, I would also recommend that you consider AD8421, AD8429 and AD8222 but these amplifier does not similar offset adjustments. However, all of this amplifiers had reference pin at which you can use to adjust the output based on the DC offsets. Also, you can also consider adding an additional gain stage after the AD8237 to achieve the gain of 4500 (Gain of 1000 for AD8237 + Gain of 45 using an precision op-amp).

    Thank you.

    Regards,
    Gilbeys 

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.