Post Go back to editing

AD8557 I want to measure current at a 0.1 ohm with one end to a load and Vcc and the other to ground. The voltage in the (-)input is in the order of 3 mV or less but I cannot amplify it

Category: Hardware
Product Number: AD8557

AD8557 I want to measure current at a 0.1 ohm with one end to a load and Vcc and the other to ground. The voltage in the VNeg is in the order of 3 mV or less but I cannot amplify it. 

When I add another resistor in series with the 0.1 Ohm resistor in the low side raising the VNeg input it, works Ok

So what is the minimum voltage I need in (-)input 

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.