Post Go back to editing

Variable Gain Implementation with AD8422 and Digital Potentiometer

Thread Summary

The user was attempting to connect a digital potentiometer (AD5293) to the Rg pins of an AD8422 amplifier to create a programmable gain. The issue was resolved by fixing a faulty SPI communication cable. No further design changes were necessary.
AI Generated Content
Category: Hardware
Product Number: AD8422ARZ, AD8422

Hello. I am working on an amplifier circuit that uses an AD8422 as the main amplifier, and I would like to know if it is possible to connect a digital potentiometer to the Rg pins so it works as a programmable resistor, for example an AD5293, to increase the gain, since I am having trouble getting it to work properly. Both devices are powered with ±12 V.

What should I take into account to implement this in case it is possible?

Thanks in advance.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.