Hello. I am working on an amplifier circuit that uses an AD8422 as the main amplifier, and I would like to know if it is possible to connect a digital potentiometer to the Rg pins so it works as a programmable resistor, for example an AD5293, to increase the gain, since I am having trouble getting it to work properly. Both devices are powered with ±12 V.
What should I take into account to implement this in case it is possible?
Thanks in advance.