KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADA4254
Recommended for New Designs
The ADA4254 is a zero drift, high voltage, low power programmable gain instrumentation amplifier (PGIA) designed for process control and industrial applications...
Datasheet
ADA4254 on Analog.com
Hello.
I have questions about ADA4254.
After reading GAIN_CAL7 on the ADA4254, GPIO3 went low approximately 500us later. Reading DIGITAL_ERR (0x03) revealed that the MM_CRC_ERR error flag in Bit1 was set.
I have a question regarding Case 2 in the “Troubleshooting MM CRC Flags” section of the ADA4254 Reference Manual.
I have set the SPI SCLK to 1MHz and the ADA4254 external clock to 1MHz. Does this correspond to Case 2?
Should I increase the SPI SCLK speed further?
Additionally, while the phases of SCLK and the external clock are each approximately aligned, could this alignment between SCLK and the external clock potentially correspond to Case 2 of the MMCRC error?

Best regards.
Hello miky,
It looks like this query is a duplicate of (+) ADA4254 GAIN_CALx Register Specification Procedure - Q&A - Instrumentation Amplifiers - EngineerZone.
I can see that one of our engineers already replied to you on the other link so I will now proceed to close this one.
Regards,
Paul