Post Go back to editing

ADA4254 GAIN_CALx Register Specification Procedure

Thread Summary

The user encountered an issue where GPIO3 goes low after several hundred microseconds when attempting to read the GAIN_CAL7 register of the ADA4254. The problem was resolved by disabling the MM_CRC_ERR error flag via the DIGITAL_ERR_DIS register, suggesting that the internal CRC operation, which runs on a 512us cycle, might be causing the error.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADA4254

Hello.

I have questions about ADA4254.

I am evaluating the ADA4254, but when I specify a read operation on the GAIN_CALx register (steps (1) to (7) below), GPIO3 goes low (error occurs) after several hundred microseconds.

Is the following procedure for specifying the GAIN_CALx register correct?
I want to know the cause of GPIO3 going low.

<GAIN_CALx Register Configuration Procedure>

(1) Set CS to Low
(2) Transmit 0x00 (Specifies writing to the GAIN_MUX register)
(3) Transmit 0x03(Gain error for G = 4 V/V × 1 V/V)
(4) Set CS to High
(5) Wait 10μs
(6) Set CS to Low
(7) Transmit 0x16 (Specifies reading the GAIN_CAL7 register)
(8) Receive the 8-bit value from the GAIN_CAL7 register
(9) Set CS to High

<ADA4254 Configuration Details>
・Set GPIO_DIR bit 3 to 1, bit 4 to 0
・Set SF_CFG (0x0C) bit 3 (FAULT_INT_OUT) to 1, bit 4 to 1
・Set bit 4 of SYNC_CFG (0x02) to 1, set bits [2:0] to 000 (÷1)
・Leave CRC at default

<Error Phenomenon Details>
Masking ANALOG_ERR (0x04) produces the same phenomenon.
Additionally, masking any of the following via DIGITAL_ERR (0x03) eliminates the phenomenon:
・Bit 3 of DIGITAL_ERR (SPI SCLK count error)
・Bit 4 of DIGITAL_ERR (SPI read/write error)

Best regards.

Edit Notes

Conditional Modification
[編集者:miky、編集時刻: 12 Nov 2025 日 2:22 AM 時 (GMT -5)]
  • Hi,

    Could you specify what you meant by "masking"? I would like to understand what errors were triggered in the analog and digital error addresses. Were there any other errors in the digital_err field aside from bit 3 and bit 4? 

    Could you also share your timing specifications? 

    Regards,

    Kristine

  • Hi,  .

    Thank you for replying.

    “Masking” means setting individual bits in the DIGITAL_ERR_DIS or ANALOG_ERR_DIS registers to 1 to disable error flags.
    We apologize, but we cannot provide the waveform. However, GPIO3 goes Low 400~500μs after step (7) below.

    (1) Set CS to Low
    (2) Transmit 0x00 (Specifies writing to the GAIN_MUX register)
    (3) Transmit 0x03
    (4) Set CS to High
    (5) Wait 10μs
    (6) Set CS to Low
    (7) Transmit 0x96 (Specifies reading the GAIN_CAL7 register) After 500μs, GPIO3 goes Low
    (8) Receive the 8-bit value from the GAIN_CAL7 register
    (9) Set CS to High


    When reading DIGITAL_ERR (0x03) this time, only MM_CRC_ERR (bit1) was set to 1, indicating an error.
    Additionally, setting MM_CRC_ERR_DIS (bit1) to 1 via DIGITAL_ERR_DIS (0x0B) resolved the issue where GPIO3 went Low.

    The internal CRC appears to operate on a 512us cycle.

    Could this be affecting the GPIO3 going Low?

    Best regards.

  • Hi miky,

    I tried a quick setup replicating the steps you provided but the error does not seem to appear on my side.

    When reading GAIN_CAL7, GPIO3 does not go low on my end.

    (SCLK - yellow, SDO - blue, GPIO3 - red)

    CRC is disabled by default so we can't really confirm that this causes MM_CRC_ERR.

    It would be helpful if you could share your timing diagrams/specs so we could take a closer look on what had occur. You can also email me at kristine.hoffman@analog.com for the files or connect with our field team if possible.

    Thanks and regards,

    Kristine

  • Hi,  .

    Thank you for your replying.


    I have sent the details via email. Could you please review them?

    Best regards.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.