Hi Team,
Is this circuit being correct? Because we are facing the issue of amplifier out is 2.25V constant from input 0V to 4V. If the input is greater than the 4V to till 32V its output increasing linearly.
Here, Issue is that the input is lesser than 4V, the output is 2.25V constant. In the simulation out is linear and there is no fixed voltage.
Is there any IC common mode supply (greater than 2.4 Volts ) which interfering in this case?
As per the simulation amplifier output is linear. But in actual circuit, getting 2.25 fixed output if the input is less than 4V.