Post Go back to editing

AD8293G80 Figure 6 and (Figure 9).

Contains AI Generated Content

Thread Summary

The user inquired about the meaning of the pink area in Figure 6 of the AD8293G80 datasheet, particularly for their application with -in = 0V and +in = +25mV to +40mV at 3.3V supply. The final answer clarified that the pink area represents the operating region for Vcc=2.7V, and the user's application falls within the linear operating region for Vcc=3.3V. The user noted that the datasheet does not explain these figures well, and most engineers might overlook the text.
AI Generated Content

The data sheet indicates that the input common mode range extends to 0V.  And the /reference input should be at least 0.8V above 0V and 0.8V below Vs+.  But what does the pink area of Figure 6 mean in the datasheet?

My input would be roughly -in = 0V and +in = +25mV to +40mV with a 3.3Vs+.

That is, I do not think I need to worry about the pink area of Figure 6 in the datasheet?

Edit Notes

AD8293 Datasheet mentioned with Figure 6.
[edited by: andrew-lohmann@home at 8:19 AM (GMT -4) on 18 Jun 2025]

Thread Notes