Post Go back to editing

AD8235ACBZ-EVALZ No Vout despite apparent proper setup

Category: Hardware
Product Number: AD8235ACBZ-EVALZ, AD8235

Hello,

I've received a new dev kit with jumpers set in default positions, which as i read it should mean the Vout, with 0V in should equal the Vref.  My Vout is zero.

  1. +VS to GND = 3.17V
  2. TP1 = 3.17V (LTC2063 enabled)
  3. TP2 = 3.17V (AD8235 enabled)
  4. Vref = 1.585V
  5. Vin = 0mV to 200mV
  6. Vout = 0V

There is no mods to the boards and all fitted components per schematic would appear to be fitted.

Things tried;

  1. Moved 2086SD jumper, Vref drops to 0V, output still 0V
  2. With 2086SD jumper to Vs (en) position AND moving 8235SD to -VS position, I do get 1.526V out

Can you assist please?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.