Post Go back to editing

AD8422 input bias during start-up

Category: Hardware
Product Number: AD8422

We are using AD8422 for DCR current sensing. Ltspice model below. However, we find when we give 7V-GND as VDD+ and VDD-, there is a bias voltage between the two input terminals of AD8422 (~100 mV range). Right now, the main power circuit is not working and the 7V input is the only supply voltage in PCB and it is only connected to AD8422. After we remove AD8422, the bias voltage returns to 0V. Is there any reason or recommendation? BTW, LTspice simulation can't repeat the phenomenon even if we try our best to match the real circuit.

Thread Notes