Post Go back to editing

Question about extra op amp input impedance

Thread Summary

The user inquired about the input impedance of the extra op amp in the AD8231 datasheet, noting that it is not specified. The final answer clarifies that the input impedance of the op amp is different from the in-amp's 10G ohm and 5 pF, and that specific information for the op amp's input impedance is not readily available.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD8231

Hello

The AD8231 datasheet does not seem to specify the input impedance of the extra op amp. The instrumentation amplifier states an input impedance of 10G ohm and 5 pF. However the op amp section of the datasheet does not specify the input impedance of the extra op amp. Is the input impedance to the extra op amp the instrumentation amplifier inputs?

Vs = 5.0 V:

Vs = 3V: