Dear Analog Team,
as I did not find information on my questions in the datasheet or application notes and in the forum, I hope you can help me on this one.
I have a signal conditioning cirucit, that consist of a source, (high-impedance) sensor, input buffer/voltage follower (AD8422), PGA, single-to-differential end converter and my ADC. My signals of interest are in the range of 0 Hz to 20 kHz. See below the setup and input voltage (positive pin to ground) and current (positiv pin) of the AD8422.
1. In the datasheet, Figure 60 shows some example applications of the sensor and also that you need to create an input bias current return path:
Hence, I wondered the following:
1)a. Is it okay to use the AD8422 as shown in my setup above? I directly connect the second input pin to ground. I did not find similar setups anywhere online/in the datasheet.
1)b. A small DC offset in voltage can be observed. Is a DC Bias resistor between the second input pin (negative pin) and ground necessary? I ask this because I sometimes see unexplainable effects, where the harmonics of my measured signal (fundamental frequency is 50 Hz) increase temporarily (I perform an FFT in my DSP after the ADC). My current guess is that moisture may change the impedance to ground in my sensor or before the AD8422. As it only measures pA, it is probably very sensitive to changes in humidity etc. Any idea/suggestion would help!
2. Would you recommend using guard rings for the input signal and if so, are there any routing recommendations for guard rings on the AD8422?
Thank you!
- changed screenshot to relevant section
[edited by: pre at 9:03 AM (GMT -4) on 3 Oct 2024]