Post Go back to editing

ad8221 ltspice error

Category: Software
Product Number: AD8221
Software Version: LTSPICE(x64) 24.0.12

Hi,

I'm simulating AD8221 in LTspice 24.0.12, the output was fine when there's no load on AD8221, but I got "singular matrix" error after adding a opamp buffer (tried ada4510/op2177/max44248) on the output node.

The simulation conditions are

Supply ±12V,  Input VCM 2.5V, Input VDiff SINE(88m 138m 1), REF 623mV, RG 4.53k.

Could you please help me understand what is causing this simulation error? Thank you!