Post Go back to editing

AD8231 vs AD8421 Selection

Category: Hardware
Product Number: AD8231

Dear Support,

I am in the design stage to choose an instrumentation amplifier from ADI to amplify a signal before 5V ADC(ADC121s051).  The instrumentation amplifier input signal has following parameters:

1. The signal has a frequency bandwidth from 100Hz to 150KHz.

2. the signal range is between 30uV ~ 30mV(peak-to-peak).

I will use 5V supply for the instrumentation amplifier and consider using the maximum gain of 128 from the AD8231 to get the maximum signal swing for the ADC input.

I have both AD8231 and AD8421 in my selection candidate list. I prefer to use the AD8231 since its wider frequency bandwidth, rail-to-rail output advantages and direct digital gain control. 

I would like to know:

a. what are the primary difference between the AD8231 and AD8421?

b. Whether it is a better choice to use AD8231 over the AD8421 for my application, or if I may have some things I miss if I choose the AD8231?

Thank you,

Lih