Post Go back to editing

Regarding the PCB layout requirements

Thread Summary

The user inquired about PCB layout requirements for the AD8228, specifically the trace widths for different pins. The support engineer confirmed that input pins (-IN / +IN, G1 / G2, REF, Vout) can use narrow traces (75um, 100um) due to being signal nets, while power pins (-Vs / +Vs) should use wider traces (300um) despite low power consumption (~20mW). The user also sought advice on trace lengths of 100mm to 200mm for -IN, +IN, and Vout, which the engineer did not address in the final answer.
AI Generated Content
Category: Hardware
Product Number: AD8228BRMZ, AD8228, AD8228, AD8228

Hello Experts,

Basic questions regarding PCB layout requirements. I would like to know which pins require what treatment in the PCB layout.

For my understanding:

-IN / +IN, G1 / G2, REF, Vout: These pins can be connected with narrow traces (75um, 100um wide traces, etc.). This is because it is a type of signal net.

-Vs / +Vs: These pins should be connected with wider traces (such as 300um traces). Because it is a type of power net. However, the power consumption is very low (~ 20mW). Full plane connections are not required.

Please let me know if there is any mistake in my understanding. Also any other critical requirements.

Reference datasheet

https://www.analog.com/media/en/technical-documentation/data-sheets/AD8228.pdf

Thanks,

Tsukada

Thread Notes

  • Hi  

    Thank you for reaching out to the team.

    I would like to ask several items below to understand the design requirements and applications better.

    • What are the intended end applications? Signal conditioning, measurements, etc..
    • What are the target supplies for this part? Do you intend to use a single or dual supply configuration?
    • What are the desired input signal and input levels for AD8228? Is this purely DC, or does it need a differential signal?

    Regarding your questions:

    Typically, I use these guidelines for board layouts:

    • Input pins: trace widths are 10 mills (~250um)
    • Supply pins:  min trace widths are 20 mills (~500um), depending on the power consumption; it can go as high as 40mills (~1000um)
    • Output should be wider than Input pins as to eliminate parasitic resistance.
    • For low-power applications, 500um is enough.
    • You might consider REF pins as supply pins if you use a source to offset your output levels.
    • Please look at pages 17 to 18 of the DS for additional layout considerations for this part. AD8228 Low Gain Drift Precision Instrumentation Amplifier Data Sheet (Rev. 0) (analog.com)

     I hope this suggestion will help you.

    Regards,

  • Hi Arsol-san,

    Your answers solved the problem I'm facing now. Also, Thank you for giving me a good perspective in the first half.

    Since we were referring to a circuit diagram created by the customer, we did not know the exact method of use. Next time, I will ask the customer for more details.

    On the other hand, there were some words that I did not understand well. Does "single or dual supply configuration" refer to the conditions for applying voltage to +Vs/-Vs? In actual application, +Vs/-Vs=+15V/-15V.

    The -IN/+IN and Vout will have a trace length of 100mm to 200mm, but if you have any concerns regarding this, it would be helpful if you could give us some advice.

    Thanks,

  • Hi  

    Correct, the dual supply configuration has a symmetrical (same absolute value) voltage being forced on +Vs and -Vs. This case is +/-15V.

    Regards,

  • Hi Arsol-san,

    Thank you for the clarification.

    Please let me know if you have any advice the following point.

    >The -IN/+IN and Vout will have a trace length of 100mm to 200mm, but if you have any concerns regarding this, it would be helpful if you could give us some advice.

    Thanks,

  • Hi  -San,

    The shorter the trace length from Input pins to a connector or source is better. To eliminate parasistics (line capacitance, impedance, etc..) that will have an effect to your signal integrity and possible voltage drop.

    Regards.