Hi,
In "A Designer’s Guide to Instrumentation Amplifiers" 3rd, p. 5-14, it recommends differential bandwidth of 10 times the signal frequency. And common-mode filter capacitors 10% the value of C2 or less. So, the common-mode bandwidth should be at least about 20 times the differential bandwidth. But latter, it says:
The common-mode bandwidth should always be less than 10% of the in-amp’s bandwidth at unity gain.
That means the differential bandwidth should be less than 0.5% of the in-amp's bandwidth at unity gain, and the signal bandwidth only 0.05% of the unity gain bandwidth, right? Won't this be too small?
Thanks.
Edit Notes
typo[edited by: diverger at 6:14 AM (GMT -4) on 14 Mar 2024]