Post Go back to editing

Role of accelerometer in minimizing noise from motion in portable cardiac monitor using AD8232.

Thread Summary

The user inquires about using the ADXL346 accelerometer to minimize motion artifacts in a portable cardiac monitor with the AD8232. The final answer suggests setting a threshold on the accelerometer to prevent heart rate measurements during high motion. For near-constant motion, such as running, the engineer recommends using x, y, and z data to detect and filter out sudden peaks in the signal.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD8232

The AD8232 datasheet has an "APPLICATION CIRCUITS" section has a subsection called "PORTABLE CARDIAC MONITOR WITH ELIMINATION OF MOTION ARTIFACTS" which says "Because the pass band is relatively wide for ambulatory applications, the ADXL346 accelerometer signal can be used to further minimize the noise introduced by the motion of the patient."

We are evaluating the AD8232 for use in our board for this portable monitor use case. Can someone please elaborate on how to the accelerometer signal should be used to minimize the movement noise from a patient?

Thanks

Parents
  • Hi  ,

    By integrating an accelerometer into the portable cardiac monitor, the system can monitor any unnecessary motion on the device especially those introduced by the patient. One can set up the accelerometer to detect any motion before measurement which could make more accurate data minimizing the noise coming from the motion of the patient. Measurement of heart rate will not occur unless the motion detected by the accelerometer is below a certain threshold value. It minimizes the noise in such a way that it prevents AD8232 from measuring the heart rate when the accelerometer detects a lot of motion.  Hope this helps.

    Regards,
    Gilbeys

  • Thanks  . Would you also have any suggestions on how to use the accelerometer to minimize noise in cases where the wearer is expected to be in near constant motion for extended periods of time, like while running?

  • Hi  ,

    Good day. You can use the x,y and z data to determine the motion of the wearer. Usually, a constant motion might cause a sudden peak in the measurement since the noise is added to the actual measurement. You can use signal processing to determine this peak and filter this out to give you the actual measurement. Thank you.


    Regards,
    Gilbeys

  • Hello,

    It appears that the above question has been answered already so I'm temporarily closing this thread. In case there are additional questions, feel free to reply to this thread. Thank you!

    Best regards,
    Paul

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.