Hello,


I am planning to configure the circuit as shown in the diagram. The input voltage ranges from 0V to 2V, and the output voltage ranges from -1V to +1V. R1 in the diagram is intended to be a variable resistor (0~20K). Are there any issues with the configuration of AD8421 and OP1177 in this setup?
Thank you.