Post Go back to editing

Dual supply and Ref voltage

Category: Hardware
Product Number: AD8421

Hello,

I am planning to configure the circuit as shown in the diagram. The input voltage ranges from 0V to 2V, and the output voltage ranges from -1V to +1V. R1 in the diagram is intended to be a variable resistor (0~20K). Are there any issues with the configuration of AD8421 and OP1177 in this setup?

Thank you.

Thread Notes

Parents Reply
  • Hi, Arsol

    First of all, thank you for your assistance.

    I want to input -1V to AD8421 Vref in order to convert the input range of 0V to 2V voltage to an output range of -1V to 1V.

    I have modified the existing circuit diagram as shown below.

    Q1. Is there any issue applying -1V to Vref?

    Q2. What additional measures can be taken to minimize noise in the AD8421 output?

    Thank you.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.