Post Go back to editing

Dual supply and Ref voltage

Category: Hardware
Product Number: AD8421

Hello,

I am planning to configure the circuit as shown in the diagram. The input voltage ranges from 0V to 2V, and the output voltage ranges from -1V to +1V. R1 in the diagram is intended to be a variable resistor (0~20K). Are there any issues with the configuration of AD8421 and OP1177 in this setup?

Thank you.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.