ADA4254 is not working properly...I have readback the part id from the ic. And Basic read write functions is working. But Couldnot use to gain purpose. Even the selftest is not working properly. Am i missing out something
ADA4254
Recommended for New Designs
The ADA4254 is a zero drift, high voltage, low power programmable gain instrumentation amplifier (PGIA) designed for process control and industrial applications...
Datasheet
ADA4254 on Analog.com
ADA4254 is not working properly...I have readback the part id from the ic. And Basic read write functions is working. But Couldnot use to gain purpose. Even the selftest is not working properly. Am i missing out something
Hi NithinAntoT,
Can you provide more details about your setup and errors you are specifically seeing in your setup? This would help us pin-point what may cause the ADA4254 to not function properly.
Regards,
Kristine
I have given input in channel 1,Pins 9 and 10,I have given a sine wave of 1khz.100mv Range. I expect out at Pin 24 and 1. But i coudnt get any. I have selected the switches A1 and A2. and opened B1 and B2.and opended C1 and C2 switch also. No result is received
What board and microcontroller do you use? And what are your supply levels?
There is issue in hardware part.Need to figure it out. Thank you for the Time.
I see. We will close this thread for now. If any new issues come up, kindly create a new thread so that we can provide support.
Thanks,
Kristine