I am using LTC2053 in the following circuit and the output waveform looks wrong. This circuit is copied from the datasheet (Precision ÷2 on page 13).

The image below shows VREF/2. It's AC coupled, 20MHz filtered, and probed using a small springy ground clip. The DC level is correct. My problem is the AC "noise". The pulses seem to be around 3kHz, which makes me suspect that the chopping frequency is coming through the output!

One complicating factor is that the power supply (5V_ISO to GND_ISO in the schematic above) has ripple. (shown below). I'm trying to solve this issue as well.

Is the noise on the power supply be causing the noise on the output of the LTC2053?
Or is the noise on LTC2053 output separate from the noise on the power supply? Is there any way to improve power supply rejection on the LTC2053 circuit?